Tornado Season: Powering Through the Strom
Tornado season usually happens from March to June. This is when weather conditions are best for these strong storms to form.
While tornadoes can develop at any time of the day or night, they are most frequently seen in the afternoon hours. Understanding tornadoes can help you to stay informed and prepared during these months when the risk is at its peak.
What is a Tornado? How They Form and Why They Cause Power Outages?
A tornado is a narrow, rotating column of air that extends from a thunderstorm to the ground.
How Does a Tornado Form?
Tornadoes form when warm, humid air near the ground collides with dry, cold air above, creating unstable weather. Strong winds at different heights cause the air to spin horizontally with violently rotating columns of air. If a storm's powerful updraft tilts this spinning air upright, it can turn into a tornado if the funnel cloud touches the ground.
Where Do Tornadoes Form?
Tornadoes happen in many areas of the country. They are most common in the United States, especially in Tornado Alley, which includes Texas, Oklahoma, Kansas, and Nebraska.
How Many Tornadoes occur each year?
About 1,200 tornadoes hit the U.S. yearly.
Tornado-related power outages can cause serious damage to homes and communities. They disrupt daily life and can lead to big financial losses. When tornadoes damage power lines, transformers, and substations, widespread blackouts can leave households without essential utilities such as heating, cooling, refrigeration, and communication. This can lead to food spoilage, health risks, and costly repairs.
Tornado Preparedness: Why You Need a Standby Generator for Power Outages
Power outages caused by tornadoes can significantly affect residences and businesses, particularly during a tornado watch, warning, or emergency. Recognizing potential outcomes is crucial.

Tornado Watch vs Warning
Tornado Watch: This means there may be severe storms. It is important to prepare for possible blackouts. Charge your devices and prepare for an outage.
Tornado Warning: Authorities issue a tornado warning when radar reports or detects a tornado. This increases the risk of power failures. High winds and flying debris can damage power lines. Seek shelter.
Tornado Emergency: Officials have declared a tornado outbreak.
Observers have spotted violent tornadoes and tornado strikes, and they expect imminent damage. This often resulting in prolonged outages that disrupt essential services, communication, refrigeration, and day to day operations. Homes may experience food spoilage, health hazards, and HVAC failures.
During tornado season, backup power is crucial for homeowners. It helps them stay safe during power outages caused by tornadoes. Stay powered with either natural gas or liquid propane as a fuel type.
Buying a backup generator, surge protectors, and emergency power solutions keeps homes safe, comfortable, and connected during bad weather.
If a tornado causes power outages from strong winds and damaged lines, your generator will turn on automatically. This keeps essential appliances like lights, refrigerators, and medical devices running.
In an emergency, when outages may last for days, a standby generator provides uninterrupted power. With heating, cooling, and communication, ensure your family's safety and comfort.
Investing in a whole-home generator gives you peace of mind. It protects you from storm-related outages, aftereffects and keeps your home running when it matters most.
How Long Do Tornado Power Outages Last? And How a Generator Helps
After a tornado, power outages can range from a few hours to several weeks, depending on the storm's intensity and the extent of damage.
In areas with minor tornado damage, power restoration may take 12 to 24 hours. However, severe tornadoes—especially EF3 to EF5 storms—can cause outages lasting several days to weeks due to downed power lines, damaged substations, and destroyed utility poles.
Rural areas typically experience longer power outages than more populated areas after a tornado event. This is due to fewer backup systems, longer distances between repair sites, and limited access for utility crews.
To prepare for extended power loss after a tornado, residents should stock up on emergency supplies, have a backup power source, and stay informed via battery-powered radios.
Understanding typical power outage durations after tornadoes helps homeowners plan ahead, reducing the risks and disruptions caused by severe weather events.
Some areas experience extended blackouts due to a combination of infrastructure damage, geographic challenges, and utility response times.
Regions with older power grids or limited redundancy are more vulnerable to prolonged outages, as repairs take longer, and alternative power sources are scarce. Rural areas often suffer longer blackouts than urban centers because of fewer power lines, greater distances between substations, and limited access for repair crews.
Severe weather events, such as hurricanes, tornadoes, and ice storms, can further delay power restoration by causing widespread damage to transmission lines and substations. In some cases, supply chain issues and labor shortages can also slow down repair efforts, extending the duration of the blackout.
Additionally, areas prone to natural disasters or high energy demand may experience rolling blackouts or grid failures, leading to extended power loss. Investing in backup power sources and staying prepared can help residents and businesses mitigate the impact of prolonged outages.

Weather any storm with Kohler.
Are you prepared to build greater resilience to withstand a tornado?
Kohler generators provide quiet and reliable backup power. They keep important appliances and systems running in your home. This includes lights, heating and cooling systems, sump pumps, computers, and much more.
Explore some of our most popular generator models and request your free quote to get started.
Keep up with tornado activity

Tornado Tracker
![HE - Hero - Modern house with large glass windows, lights inside, on a rainy night.
Why Kohler [Article 17]
whyKohlerhero.jpg](/_next/image?url=https%3A%2F%2Fimages.ctfassets.net%2Fzlhl2y58oyef%2F12KK9JhccBxtaw8KpVp4iI%2F0b519f57a16121759d5b9ec7cb378df4%2FwhyKohlerhero.jpg&w=3840&q=100)
Doppler Radar
![Modern architecture white house, under a clouded night sky, lit by outside spotlights and featuring a Kohler Generator nestled up against the base of the home.
DAM # aab96124
Articles: [1] Does Generator Work Home Type
Size changed to 16:9 ratio](/_next/image?url=https%3A%2F%2Fimages.ctfassets.net%2Fzlhl2y58oyef%2F4s7NIlq6gWZPkjXVoPPLdz%2Fdf49e6704e563b7bb5f5baa5f9e886c2%2Faab96124_rgb.jpg&w=3840&q=100)