Skip to main content

Winter weather can change in strength and severity each year. It brings different conditions that can affect daily life. Having KOHLER backup power is a good way to feel safe and have peace of mind during winter storms and power outages.

Many factors influence weather and understanding it requires a closer look at several key elements. Regional location plays a crucial role. Different parts of the world have unique weather patterns and features. These features can greatly influence local weather conditions. Climate patterns are another critical factor. Long-term trends in temperature, precipitation, and seasonal changes can shape the environment. The specific weather conditions during a given season can greatly influence outcomes. Short-term weather events, such as a snowstorm, can change the weather in your area. These events include heavy snow, ice storms, and frigid temperatures.

Prepare for the cold – Ensure your generator is winter-ready! Check your unit’s spec sheet for heater kit recommendations when temperatures drop below 32°F (0°C). Need a cold weather kit? See our options here or contact your local dealer.

Winter Weather Generator Tips and Maintenance

Performing generator maintenance during cold weather is essential to ensure it remains in good working condition. Proper care can help prevent issues that might affect its performance. This ensures it is ready to provide power when needed. By taking the necessary steps, you can keep your generator functioning efficiently throughout the colder months.

Clear Air Intakes and Exhaust Vents:

  • Keeping air intakes and exhaust vents clear of snow is essential for generator efficiency. Snow buildup for extended periods can restrict airflow, causing your power system to overheat and shut down. 

  • Regularly removing snow can help maintain proper function and extend the generator's performance during winter. 

Image of a Kohler home generator outside of a house during a blizzard.
Image of a brown house with its light on, and a Kohler home generator outside, in a snowy landscape.

Keep Access Paths Clear:

  • Maintaining clear and unobstructed access paths to your generator is crucial.  

  • This ensures that you or maintenance personnel can easily reach the generator for routine any necessary maintenance. Also, having clear paths for access allows for quick oil refueling. This is important to keep the generator running during long periods of use. 

  • In case of any troubleshooting needs, unobstructed access allows technicians to diagnose and address issues promptly. This minimizes downtime and ensuring the generator remains in optimal working condition. Regularly check and clear any obstacles that might block these paths to maintain a safe environment around your generator. 

Checking Your Oil:

  1. Safety First: 
    Ensure the standby generator is not running and that it is switched off. If you are unsure how to verify this contact your local service provider. 

  2. Check Oil Level: 
    Locate the engine oil dipstick. Using a clean rag, remove the dipstick and wipe off the oil. Reinsert the dipstick and remove it again to check the oil level. If the oil level is low, you may top off with KOHLER 5W30 full synthetic engine oil. 

  3. Refill Carefully: 
    Add oil in small increments, checking the level frequently to avoid overfilling. 

*Please see your generator's owner manual for more detailed instructions and recommendations. 

Bottle of KOHLER oil being poured.

10 Winter Storm and Cold Weather Safety Tips

  • Stay Informed
    Monitor your local weather reports and pay attention to warnings and advisories.

  • Dress in Layers
    Wear warm and moisture wicking layers. Be sure to use a waterproof outer layer to stay dry and insulated from snow or freezing rain. Keep in mind the wind chill factor and dress appropriately.

  • Avoid Frostbite and Hypothermia
    Limit outdoor exposure and stay indoors during extreme cold weather.

  • Prep Your Home
    Let faucets drip during extreme cold to ensure water flow to help prevent freezing. Inspect and seal any drafts near windows or doors. Be sure to test fire alarms and carbon monoxide detectors if using space heaters, fireplaces or additional portable generators.

  • Winterize Your Vehicle
    Check tire pressure and tread while also keeping your gas tank half full to prevent freezing.

  • Drive Safely
    Increase your follow distance from other vehicles on snowy and icy roads. Avoid sudden breaking or acceleration to prevent sliding.

  • Keep an Emergency Kit Ready
    Include essentials such as:
    I. Battery Powered Flashlights and Spare Batteries
    II. Non-perishable Foods
    III. Bottled Water
    IV. Extra Blankets
    V. See our preparedness article here to learn more.

  • Protect Your Pets
    Bring your pets indoors and provide warm bedding or other heat sources in case of extreme cold temperatures. Wipe paws after being outside to remove ice as well as salt and chemicals from de-icing products.

  • Shovel Safely
    Warm up before and after attempting to shovel heavy snow. Be sure to take frequent breaks if the temperature is extremely low to avoid fatigue.

  • Stay Hydrated
    Stay hydrated even if you don't feel thirsty, cold weather can cause dehydration without obvious signs.

Stay up to date with winter storm watches, winter storm warnings and extreme cold maps: National Weather Service.

KOHLER Home generator written on the corner of the image with a man working on a laptop.

Defend Against Unpredictable Weather | Wendell's Testimonial

"The weather has been more extreme and a little more erratic in the past 10 years."

Get Performance You Can Count on, Again and Again.

For backup power that keeps you in motion, even during an outage, choose a Kohler home generator. Request your free quote today to find the right model for your home.

Read More About Storm Preparation

5 Post-storm Safety Tips: Protect Yourself and Your Home

READ MORE

Plan to Protect Your Home and Family

READ MORE

How to Make Emergency Preparedness Kid-Friendly

READ MORE

How to Create a Hurricane Evacuation Plan

READ MORE

Home Energy Help & Support

Call Our Team

1-800-544-2444

Kohler Home Energy Customer Care Center
Monday - Friday 7:30am - 5:00pm (CT)

A woman with headphone in front of a computer in a support call. Author: © ty - stock.adobe.com